A Learning in Motion Top Ten SelectionThe Field Trips SiteSubject Area: Teacher Pick Address/URL: http://www.field-trips.org Description: This site has developed a user interface enabling classes to go on virtual field trips in exotic areas of the world. These annotated field trips take students to some of the best web sites on each trip subject. Listed are also additional teacher's resources for each of the trips. The learning format is fun and easy to use, making the use of internet in the classroom simple. How You Can Use This Source:
Go to The Field Trips Site.
© 2004 Learning in Motion, Inc. |