A Learning in Motion Top Ten SelectionMr. Pitonyak's Pyramid PuzzleSubject Area: Teacher Pick Address/URL: http://wcvt.com/~tiggr/ Description: Mr. Pitonyak's Pyramid Puzzle page is an outstanding example of a compelling problem, where real-life tasks and technology are seamlessly integrated into the middle school math curriculum. It simulates the work construction contractors would have to do when submitting a bid. Students are divided into teams and each team member is assigned a well-defined job. All materials required for submittal are clearly described on this web page. An Internet reference list is also included to make the research easier. How You Can Use This Source:
Go to Mr. Pitonyak's Pyramid Puzzle. © 2004 Learning in Motion, Inc. |