home                     services                     products                     about us          
logo
overview
educational
perspectives
primary
math test
development
module
Resources for the Hearing Impaired

Educational Communication Perspectives:


I. Oral Communication Perspective:
In general, oral programs emphasize use of spoken language and listening. They are taught through oral/verbal instruction or the use of an oral interpreter. No sign language is used. Oral programs may use one or more of the following strategies/tools for instruction: speech/audiological training, assistive-listening devices, development of listening skills. Many oral programs are private schools, however there are some public oral programs. Modifications to audio and the addition of captioning are the types of modifications that should be considered for this population.

Back to top...

Modifications to Consider:

A. Captioning

  • Basic captions: A basic captioning modification would consist of text appearing at some designated place on the screen (preferably the bottom of screen). The text would follow every spoken word by the characters in the program. This feature would allow the user to use their residual hearing in conjunction with the printed word. This would reinforce listening skills as well as offer read-along practice.

  • Highlighting of words tied to audio
    An additional modification to captioning could include a "highlighted" captioning feature. As the words are spoken the individual words would be highlighted so that the user could "read-along" word by word with the character. Such a modification would offer an additional level of support in addition to the benefits mentioned above.

Back to top...

B. Sound levels
The user should have the option of increasing or decreasing the volume of the characters' voices, sound effects and any other auditory information presented in the program.

 

C. Frequency levels
Since deaf children tend to have losses in the higher frequency range, an investigation should be made regarding the alteration of the acoustical information in the software. A possible modification could be the ability to adjust the frequency of the characters' voices, sound effects and any other auditory information (normal sound vs. lower frequency sound). The teacher or individual user could set this feature as part of a user profile.

Back to top...

D. Visual clues:

  • Blinking/highlighting:
    Blinking or highlighting objects can be used as a way to draw the user's attention to important icons or other information. The use of blinking/highlighting may be used as a way of indicating what object the person is to "click" on. Blinking/highlighting may also be used to draw attention to objects when instructions are being given.

  • Animations
    Animations can be used to demonstrate how to complete a task. A character in the program may move about the screen as they are explaining the directions. The animations can be used with other visual clues, such as blinking/highlighting.

Back to top...


II. Manual Communication Perspective:

The manual communication perspective contains several different views on communication. One of these views is the bilingual/bicultural philosophy which recognizes American Sign Language (ASL) as the natural language of the deaf. They use ASL for instruction and conceptual understanding of material. In addition, they teach English as a second language for reading and writing. The child is considered "bilingual" when they have mastered both languages. The "bicultural" aspect of this philosophy is that they teach both hearing and deaf culture. They teach deaf children to be proud of their deaf heritage. They expose the children to deaf adult role models. Other manual communication programs may use a variety of different types of sign language including Pidgin Signed English (PSE), Signed English (SE), and Signing Exact English (SEE). Often these types of programs use spoken English in conjunction with signing (see Total Communication Perspective below).

Back to top...

Modifications to Consider:

A. Sign Language
A decision needs to be made regarding what type of signing will be included in the program. This will likely depend on whether different types of signing are available either through Signing Avatar, video technology or other signing animation. There are four types of signing that should be considered: American Sign Language, Pidgin Signed English , Signed English and Signing Exact English. Currently, Signing Avatar uses PSE (also known as Conceptually Accurate Signed English) and SE. Each type of signing has its own audience. However, some forms of sign language are more accessible to a greater number of signers. Modes of signing are not completely isolated from one another. The different types of signing follow more of a continuum rather than isolated modalities. The less "English" structure the signing contains, the closer it falls to ASL on the continuum. The more "English" structure the signing contains the closer it falls to SEE.

Back to top...

  • American Sign Language (ASL)
    ASL is the natural language of the Deaf and also the most used form of communication among the Deaf. However, if a signing module is included in a program, it must be understood that ASL signs will not match the speaker word for word. ASL has its own grammatical structure (different than English). ASL tends to be a visual or concept based way of communication. Users who are only familiar with SEE signs may have a difficult time understanding a pure ASL model. Signing Avatar may be adapted to sign in an ASL mode.

  • Pidgin Signed English (PSE)
    PSE is not a specific form of signing. The term PSE is used to refer to signing that is in the middle of the continuum of signing. PSE is often some form of combination of ASL and a manually-coded English. PSE is a likely choice for the signing module. A decision will need to be made as to if the PSE signer will use ASL signs in an English word order (Conceptually Accurate Signed English, CASE) or use more of a manually-coded English like SE. It is likely that most users who sign will be able to follow a signer using a form of PSE. It can be matched closely to the current spoken English audio on a program. Currently, Signing Avatar offers PSE/CASE as an avatar option.
  • Back to top...


  • Signed English (SE)
    SE is similar to SEE sign. It follows closely to English grammar and structure. However, it has fewer supplementary signs for endings of verbs and other words. SE is also one of the forms currently available through Signing Avatar.

  • Signing Exact English (SEE)
    SEE, like ASL, is probably not the ideal choice to include in a program unless all other forms of signing are also included as options. SEE has a smaller audience of users and educational programs as compared to PSE /ASL based users and educational institutions. SEE is a form of manually-coded English. It tends not to be as visually conceptual as other modes of signing. SEE follows English grammar exactly by using supplementary signs for endings such as -ing or -ed. It would be difficult for ASL signers to follow SEE signing.

B. Captioning (see Oral Communication Perspective)

C. Sound levels (see Oral Communication Perspective)

D. Frequency Levels (see Oral Communication Perspective)

E. Visual clues (see Oral Communication Perspective)

Back to top...


3. Total Communication Perspective:
The total communication philosophy has many variations. In general, they use a combination of various methods and approaches to meet the individual child's needs. A combination of sign language, fingerspelling and spoken English is often used. The type of sign language used may vary: Signed Exact English (SEE), Signed English (SE), American Sign Language (ASL), or Pidgin Signed English (PSE). In addition, some programs may include the use of Cued Speech to assist the child in English access.

Modifications to Consider:

A. Sign Language (see Manual Communication Perspective)

  • American Sign Language (ASL)
  • Pidgin Signed English (PSE)
  • Signed English (SE)
  • Signing Exact English (SEE)

B. Captioning (see Oral Communication Perspective)

C. Sound levels (see Oral Communication Perspective)

D. Frequency Levels (see Oral Communication Perspective)

E. Visual clues(see Oral Communication Perspective)

Back to top...

 

 

This material is based upon work supported by the National Science Foundation
under Grant No. 0079350. Any opinions, findings, and conclusions or
recommendations expressed in this material are those of the author(s) and do
not necessarily reflect the views of the National Science Foundation.